This is a brief description for the files in this folder

distkit.OMEGASOFT IR OS5xx Access.1.x.x.zip (8.97mb)- Free user interface software for OMEGA OS530E
Series of Infrared Thermometer. The file is a zip file. Software Version will be
shown during installation.

*Operation reference: Omega Handheld Infrared Thermometer User's Guide(OS530E series), 
Document No. M4088-0705-OS530Series.pdf

-----------------------------------------------------------------------------------------
1. About OMEGASOFT IR OS5xx Access

OMEGASOFT IR OS5xx Access is a free software.

You may find the latest version of it at Omega Engineering, Inc. home page and
the following sites:

ftp://ftp.omega.com/public/TEMPERATUREGroup/products/os5xx
(These addresses may be changed in future.)

-----------------------------------------------------------------------------------------
2. Requirements

Supported operating systems: Windows 2000 + Service pack 3

Following minimum requirements: 256 MB RAM

Hard disk with a minimum of 20 MB free space

-----------------------------------------------------------------------------------------
3. Installation from Omega website

1) If you have installed an old version of OMEGASOFT IR OS5xx Access, just install over
the old version. No need to uninstall.

2) Download the OMEGASOFT IR OS5xx Access setup zip file from the website to your computer
at selected directory.

Download will begin automatically, and you will receive prompts asking you if you want 
to proceed.

3) After download completed, Go to the directory where the setup files are Downloaded and
unzip them to your desire directory. Double-click on Setup.exe from that directory and 
then follow the installation instruction.

4) When the installation finishes, run the program to be sure it behaves as expected. 

-----------------------------------------------------------------------------------------