Software for the TVS-1100

System Requirements:
Use a PC with a minimum of 128 MB of memory and one of these operating
systems: Windows 98, 2000, XP, NT, or ME. To maintain an acceptable level of
safety, the host computer should comply with the requirements of UL/CSA/IEC
60950.

Software installation
To install the software, the following steps must be taken:
1. Install the Visa300runtime.exe by double-clicking the file. This file enables the
executable TVS-1100 software to communicate through the RS232 serial port.
2. Install the TVS-1100 software by double-clicking on TVS-1100/installer/setup.exe.
3. Place the file called TVS-1100 calibration data on the C root directory.