Omega .NET Products API README
================================

This package contains a .NET dll that allows you to communicate with your Omega
digital sensors. The assembly is located in the "Lib" folder. There is also an
example application illustrating how to use the assembly in your .NET project.
This assembly currently supports the following products:

* PX409-USB
* PX409-USBH
* TJ-USB
* UTC-USB
* RH-USB
* IR-USB
* LC411-USBH

Examples
---------------

### PX409-USBH Streaming Example ###

This is an example that allows a user to choose from the detected PX409-USBH
sensors and begin streaming measurements to the console. By replacing
"PX409Usbh" with "LC411Usbh" this example can detect and stream from LC411-USBH
sensors.

Troubleshooting
---------------

If you're having issues opening the .chm help file, you may have to "unblock"
the file.

1. Right-click on the .chm file and choose properties
2. Near the bottom of the properties window, click the "Unblock" button.