Dashboard Software 

DASHBOARD 1.00.11-2 for Windows (XP, Vista, Win 7, Win 8,Win 10 compatible with 32bit/64bit systems) 

Date: 11/30/2016  

Features: 
 Lower CPU and RAM usage on computer.  
 Avoid creating more than one connection for all the devices.  
 Better hear beat checking scheme. 
 Added support for WW-ED Wi-Fi device(beta).  
 Improved the reconnecting function for ZW-REC 

Issues: 
 must backup if you want to un-install (see IMPORTANT note below).

============================
IMPORTANT notes for DASHBOARD 1.00.11-2 INSTALLATION:
Please backup your C:\ProgramData folder if you want to uninstall any previous version of Dashboard (1.00.8 and earlier).
In order to prevent the software from deleting files and folders in C:\ProgramData caused by un-installing
the previous versions of Dashboard, please upgrade the software to this version without un-installing the
previous version on the computer. 

By doing upgrading and running the installer packet directly, the program will skip the cleanup step for the ProgramData folder, 
and the uninstallation of Dashboard 1.00.11-2 will not delete the files/folders in ProgramData folder. 

NOTES for firmware versions: 
============================
*The zCDR with EIP only works with Dashboard 1.00.6 (the previous version), not the latest 1.00.11-2.  
To check if your zCDR has the EIP, check the firmware version, if it is 3.0 or greater, it is an EIP based zCDR. 
You can check the Firmware version listed on zCDR Homepage.  

**The UWTC-REC3 with EIP only works with Dashboard 1.00.6 (the previous version), not the latest 1.00.11-2.  
To check if your UWTC-REC3 has the EIP, check the firmware version, if it is 3.2 or greater, it is an EIP based UWTC-REC3.
You can check the Firmware version listed on UWTC-REC3 Homepage.

==========================================================================================================
==========================================================================================================

Version 1.00.10.0 for Windows (XP, Vista, Win 7, Win 8,Win 10 compatible with 32bit/64bit systems)  
Date: 09/21/2016 
Features:
 Fixed the issue of downloading the current data file on the Data tab. 
Issues:
 This version 1.00.10 does not support the EIP based zCDR, please use 1.00.6 with EIP based ZCDR(firmware 3.0 or up on the homepage of zSeries coordinator).
 This version 1.00.10 does not support the EIP based UWTC-REC3, please use 1.00.6 with EIP based UWTC-REC3(firmware 3.2 or up on the home page of UWTC-REC3).
 Please backup your C:\ProgramData folder if you want to uninstall any previous version of Dashboard( 1.00.8 and earlier). In order to prevent the software from deleting files and folders in C:\ProgramData caused by uninstalling the previous versions of Dashboard, please upgrade the software to this version without uninstalling the previous version on the computer. By doing upgrading  and run the installer packet directly, the program will skip the cleanup step for the ProgramData folder. And the uninstallation of Dashboard 1.00.9 does not delete the files/folders in ProgramData folder. 

==========================================================================================================
==========================================================================================================

Version 1.00.9.0 for Windows (XP, Vista, Win 7, Win 8,Win 10 compatible with 32bit/64bit systems)  
Date: 07/08/2016 

Features:
 Fixed the issue that some computers may lose files and folders in C:\ProgramData folder after uninstall the software. 
Issues:
 This version 1.00.9 does not support the EIP based zCDR, please use 1.00.6 with EIP based ZCDR(firmware 3.0 or up on the homepage of zSeries coordinator).
 This version 1.00.9 does not support the EIP based UWTC-REC3, please use 1.00.6 with EIP based UWTC-REC3(firmware 3.2 or up on the home page of UWTC-REC3).
 Please backup your C:\ProgramData folder if you want to uninstall any previous version of Dashboard( 1.00.8 and earlier). In order to prevent the software from deleting files and folders in C:\ProgramData caused by uninstalling the previous versions of Dashboard, please upgrade the software to this version without uninstalling the previous version on the computer. By doing upgrading  and run the installer packet directly, the program will skip the cleanup step for the ProgramData folder. And the uninstallation of Dashboard 1.00.9 does not delete the files/folders in ProgramData folder. 

==========================================================================================================
==========================================================================================================

Version 1.00.8.2 for Windows (XP, Vista, Win 7, Win 8,Win 10 compatible with 32bit/64bit systems)  
Date: 03/31/2016 

Features:
 Added the option to trust all the certificates for the SSL
 Fixed the problem that when devices get lost, it dooes not connect it again. 
Issues:
 This version does not support the EIP based zCDR, please use 1.00.6 with EIP based ZCDR(firmware 3.0+).
 This version does not support the EIP based UWTC-REC3, please use 1.00.6 with EIP based UWTC-REC3(firmware 3.2+).

==========================================================================================================
==========================================================================================================

Version 1.00.7.2 for Windows (XP, Vista, Win 7, Win 8,Win10 compatible with 32bit/64bit systems)  
Date: 03/11/2016 

Features:
Added the support for the new ZW-REC devices
SSL support for ZW-REC
Using one solid TCP connection to keep sending the commands
It can detect the LostED for end devices and send the email alarm 
Changed the algorithm to calculate the backend updating rate for coordinators. 
Solved some display bugs on the alarm webpages
Removed the server log in this version
Issues:
 This version does not support the EIP based zCDR,please use 1.00.6 with EIP based ZCDR(firmware 3.0+).
 This version does not support the EIP based UWTC-REC3, please use 1.00.6 with EIP based UWTC-REC3(firmware 3.2+).

==========================================================================================================
==========================================================================================================

Version 1.00.6 for Windows (XP, Vista, Win 7, Win 8, compatible with 32bit/64bit systems)  
Date: 12/09/2015 

First release of this sofotware

Feature:
Real time data logging through network globally
Monitoring readings from 100+ of Omega devices at the same time
Charting for real time or recorded data 
Sending email or text message alarm
Downloading data from webpage


It supports all the Omega iServer based Ethernet products including:
iServer Temperature Transmitters/Recorders:iTCX-W, iTCX-D, iSD-TC
iServer Temperature and Humidity Transmitters/Recorders: iTHX-SD, iTHX-W, iTHX-W*, iTHX-M, iTHX-D, iSD-TH
iServer Barometric pressure and Temperature Transmitters/Recorders:iBTX-SD, iBTX-W, IBTX-M, IBTX-D
iServer Barometric pressure, Temperature and Humidity Transmitters/Recorders:iBTHX-W, iBTHX-*
IEEE 802.15.4 wireless based products:zSeries,  UWTC series(with UWTC-REC3), and new ZW series(release soon)
iServer based controllers/transmitters:Platinum,DPI , CNi, iLD, iR2,  iDRN, iDRX (these products need to be ordered with Ethernet option)
IEEE 802.11 Wi-Fi based wSeries transmitters