Omega.Daq .NET framework README


Requires at least .NET 2.0 and a CLS-compliant .NET programming language.  Supports C#, Visual Basic .NET, and Visual C++.
Depends on the FTDI Chip .NET framework FTD2xx_NET.dll, which is included.

---------------
GETTING STARTED
---------------
1.) Read the OVERVIEW below.
2.) Examine the included sample code.  The C# and VB samples are functionally equivalent.  
The sample code demonstrates how to detect devices, and how to receive data using Easy and Standard modes.
3.) Refer to the included help file for a complete API reference. Copying the Omega.Daq.xml file to your project when you include Omega.Daq.dll will provide Microsoft Intellisense support in Visual Studio.


--------
OVERVIEW
--------
OMB-DAQ-USB devices are represented by instances and subclasses of the Device class. Devices can be searched for with Device.FindConnectedDevices().
A Daq2401Demo object (a subclass of Device) is provided for testing without any connected hardware.  

The Omega.DAQ framework supplies two modes of reading data from the device: "Easy" and "Standard".

Easy mode is a very simple, but slower method of obtaining data.  It handles the details of setting up the device and receiving data.  See the Device methods EasyRead() and EasyScan().
Standard mode requires more function calls and setup, but allows more customization and faster, more direct access to the data.

The sample code demonstrates EasyScan(), EasyRead(), and the Standard mode for both a Daq2401Demo device and a real device, if connected.