This is a brief description for the files in this folder

xx-xx-xx-1xx.zip (9mb)- Free user interface software for OMEGA CTXL recorder Series.
The file is a zip file. Software Version will be shown during installation.

-----------------------------------------------------------------------------------------
1. About OMEGASOFT CTXL-PH Access

OMEGASOFT CTXL-PH Access is a free software.

You may find the latest version of it at Omega Engineering, Inc. home page and
the following sites:

ftp://ftp.omega.com/public/TEMPERATUREGroup/products/CTXL
(These addresses may be changed in future.)

-----------------------------------------------------------------------------------------
2. Requirements

Supported operating systems: Windows 2000 + Service pack 3, Windows XP, Windows 7, Windows 8/8.1

Following minimum requirements: 256 MB RAM

Hard disk with a minimum of 20 MB free space

-----------------------------------------------------------------------------------------
3. Installation from Omega website

1) If you have installed an old version of the program, just install over
the old version. No need to uninstall.

2) Download the OMEGASOFT CTXL-PH Access setup zip file from the website to your computer
at selected directory.

Download will begin automatically, and you will receive prompts asking you if you want 
to proceed.

3) After download completed, Go to the directory where the setup files are Downloaded and
unzip them to your desire directory. Double-click on Setup.exe from that directory and 
then follow the installation instruction.

4) When the installation finishes, run the program to be sure it behaves as expected. 

-----------------------------------------------------------------------------------------

4. Revision history

- 1.2.1 Updated user interface to specyfiy the log file at the beginning of logging process.
	Updated paper chart pen configuration menu.
	Muted intro sound according to "Audible indications" settings.
	Improved USB communication in order to address IO timeout error.
- 1.2.2 Added support for Windows 8/8.1